POWERING PRODUCTION

W.R. Grace
W.R. Grace

W.R. Grace Depends On Cogeneration To Offset Energy Costs

Customer: W.R. Grace / Davison Chemical Division

Location: Baltimore, Maryland

Customer Business Issue: Energy savings, reduced emissions

Solution: 3520H generator sets (2)

Cat® Dealer: Carter Power Systems

 

of

W.R. Grace commissioned the CHP plant in November 2019, installing two Cat® 3520H generator sets, each with an oxidation catalyst and a selective catalytic reduction system, to power the system.

of

Combined, the two generator sets product about 5 MW of electric power, offsetting about 40 percent of the plant’s annual power consumption.

of

“The CHP system is a key tool for our plant to remain competitive, reduce our GHG emissions, and improve our long-term sustainability goals.” – Richard Martin, project manager for W.R. Grace.

of

Benefits of the CHP system include an estimated annual energy savings of $1.2 million, increased reliability of its electrical supply, and expected annual greenhouse gas reduction of 14,415 tons CO2e.

POWER NEED

The Curtis Bay facility of W.R. Grace & Co. is located on an industrialized peninsula in South Baltimore, Maryland. At one million square feet, Curtis Bay is the largest of the conglomerate’s 22 manufacturing plants, with six production facilities that manufacture hundreds of products within four general product lines.

All four W.R. Grace business units are represented, including Material Technologies, Specialty Catalysts, Refining Technologies and Advanced Refining Technologies. The products that originate from the Curtis Bay plant are used to make anything from pharmaceuticals to toothpaste, gasoline, and bottles and cans.

Before W.R. Grace acquired the facility in 1943, manufacturing at this location began in 1910 making sulfuric acid, then fabricating munitions during World War I; and silica gel throughout World War II as a dehydrating agent to protect shipments from the damaging effects of air and moisture. Today, the facility makes catalysts and silicas.

The W.R. Grace plant operates 24/7. Electrical demand varies by approximately 15 percent on a monthly basis, and monthly electrical consumption varies by up to 30 percent. Monthly natural gas usage varies by up to 23 percent depending on process operation.

To meet its power demand, Curtis Bay plant uses both electricity and natural gas supplied by Baltimore Gas & Electric (BG&E). The plant has a 14.7 MW peak demand—but has an average load of 12 MW—and uses approximately 94,430,830 kWh/year. Curtis Bay uses natural gas to directly supply process load and also supply boilers used for steam and hot water throughout the facility.

Aging infrastructure is an ongoing challenge at Curtis Bay, as old utility feeds and transformers occasionally go down, says project manager Richard Martin.

“We try to maintain them as best we can. It’s a big facility and we have a crew dedicated to making sure that things are maintained and respond to any shutdowns,” Martin says. “Loss of power is a big issue on this site—it shuts down basically all of our production, and if we’re not producing product, we’re not making money.” 

SOLUTION

In late 2016, Grace began the planning process to install a combined heat and power (CHP) project, subcontracting both the design and construction of the CHP plant. Ultimately, the plant was commissioned in November 2019, and includes two Cat® 3520H generator sets supplied by Cat dealer Carter Power Systems that are located in a fit-for-purpose building. Each engine is equipped with an oxidation catalyst and a selective catalytic reduction (SCR) system to meet stringent environmental criteria.

“We consume an average of about 12 megawatts of power, with redundant distribution from what we call our horseshoe,” Martin says. “It’s our main feeding facility where the power from the utility enters the site. So, we were looking to offset some of that power and reduce our operating costs by utilizing cogeneration with the Cat gensets.”

Combined, the two generator sets produce about 5 MW of electric power, offsetting about 40 percent of the plant’s annual power consumption.

The heat recovery system was designed to receive 450 gpm of city water at temperatures varying from 47°F in the winter to 70°F in the summer, and deliver hot water at about 130°F to the plant instead of heating it with steam. The water flows through two heat exchangers in series, with the first exchanger pulling heat from the first-stage aftercooler; and the second exchanger pulling heat from the jacket water, lube oil cooler, second-stage intercooler, and exhaust heat. The hot water is stored in 10,000-gallon insulated tank and used in a process stream.

“We recognized the advantage of recovering heat that we can use in a wash media in our manufacturing process,” Martin says. “We previously heated up the water using the onsite steam boilers, but now we can use the hot water generated from our CHP system to offset much of that load.”

RESULTS

The benefits to Curtis Bay plant are numerous. Since the CHP system began operating, utilization of the boilers to heat the water has dropped significantly, Martin says. Thermal offset of about 10 percent of its annual natural gas consumption, including boiler efficiency loss, has been realized. The overall efficiency of the CHP system is about 75 percent.

Other tangible benefits include:

  • An estimated annual energy savings of $1.2 million
  • Increased reliability of its electrical supply
  • Expected annual greenhouse gas reduction (GHG) of 14,415 tons CO2e

Financial incentives helped make the project feasible. Grace received a Maryland Energy Administration CHP Incentive Grant of $500,000, and potential BGE CHP Incentive Grants of approximately $4 million based on genset utilization. Total payback on the project is expected to be realized in less than five years from its inception, Martin says.

“The CHP system is a key tool for our plant to remain competitive, reduce our GHG emissions, and improve our long-term sustainability goals,” Martin says.

All scheduled maintenance—including fluid sampling—is handled through a service contract with Carter Power Systems, which is located 15 minutes’ drive from the Curtis Bay facility.

“Nobody likes to see these units down, and if they’re not running I get phone calls,” Martin says. “The folks at Carter are responsive, and I’ve been happy with them. Their main technician, Mike, is a great guy. He really knows these Cat generators and he’s been very helpful to us. So, we’re glad that we’re in partnership with him and the Carter Cat team.”

Download the Power Profile

 

Featured product

  • G3520H
    Continuous Rating
    2519 / 2500 ekW @ 1.0pf
    2519 / 2500 ekW @ 1.0pf
    Fuel Type
    Natural Gas, Hydrogen Blend (up to 25%)
    Natural Gas, Hydrogen Blend (up to 25%)
    Maximum Electrical Efficiency
    45.30%
    45.30%

    G3520H

    From natural gas to biogas, coal mine gases, or hydrogen fuel blends to support combined heat and power (CHP), emergency power, and local grid support applications, Caterpillar has a wide range of reliable gas power solutions.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Cat Electric Power now has two tools available for sizing gensets in any application. 

Size Now
genset sizing
genset sizing

Manufacturing

When your lines aren't moving, you're not making money. You need power that will keep you in production and keep you efficient. Cat® standby generator sets run with low owning and operating costs. We’re helping you maximize profit by minimizing electrical expenses.

View Manufacturing Page
manufacturing
manufacturing

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.