STABLE, CLEAN, UNINTERRUPTIBLE POWER

Docler
Docler

Reliable Standby Power Supply, Maximum Uptime

Customer: DoclerWeb

Location: Budapest, Hungary

Scope of engine use: Cat® 3516B-HD 2500 kVA diesel generator set

Cat Dealer: Huntraco

 

of

Cat® 3516B-HD

of

DoclerWeb provides co-location, server hosting and application hosting to hundreds of customers, allowing them to offer complex Internet portals, databases or multimedia content in a safe, high-standard technical environment

Power Need

Located in the capital city of Budapest, Hungary, DoclerWeb provides co-location, server hosting and application hosting to hundreds of customers, allowing them to offer complex Internet portals, databases or multimedia content in a safe, high-standard technical environment to a large number of visitors from all over the world.

Power outages – even minor voltage sags or spikes lasting less than one second – can cause sensitive equipment to falter, forcing the company to shut down its data servers and halt all business. To meet the company’s uptime requirements, DoclerWeb needed standby power from an integrated system to ensure a highly reliable continuous electrical power supply for the data center and other company facilities.

Solution

DoclerWeb turned to the local Cat® Dealer Huntraco for an integrated power system including a Cat 300 Series Uninterruptible Power Supply (UPS) unit and a Cat 3516B-HD 2500 kVA diesel generator set. The Cat UPS provides up to 750 kVA of power and, when combined with the generator set, provides stable, clean and quality power for the DoclerWeb data center and the rest of the company’s facilities.

“DoclerWeb is open to innovative solutions, and they used this new installation to compare the operational costs of their traditional battery-powered UPS with a new Cat UPS,” said Balazs Sarkadi, the sales engineer for Huntraco Hungary. “DoclerWeb emphasizes high-quality, reliable technologies, and they do not consider any ‘no name’ brands.”

The radiators for the engine were installed on the roof of the building as opposed to the typical placement in the generator room, leaving space for an additional generator set that will be needed as the data center expands.

“Even though DoclerWeb investigated other brands, only Huntraco and Caterpillar were able to offer a customized solution that included the installation of a cooling system on the roof,” Sarkadi said.

Results

The standby system for DoclerWeb was installed and commissioned on schedule with the excellent local support of Huntraco, and DoclerWeb now operates the highest performance Cat diesel generator set and first Cat UPS in Hungary.

Download the Power Profile

Featured Products

  • 3516B (50 Hz) 2500 kVA with Upgradeable Package
    Standby Rating
    2500 kVA
    2500 kVA
    Prime Power Rating
    2275 kVA
    2275 kVA
    Emissions/Fuel Strategy
    Low Fuel, Low Emissions
    Low Fuel, Low Emissions

    3516B (50 Hz) 2500 kVA with Upgradeable Package

    Producing reliable power from 2000 to 2500 kVA at 50 Hz, our 3516B diesel generators are made to meet your mission critical, continuous, standby and prime applications. We've designed each to ISO 8528-5 transient response requirements and to accept 100% rated load in one step. Cat® generators offer both low fuel consumption and low emission systems.
    FAQ
    Q. Does this generator comply with ISO 8528 guidelines?
    A. Yes, the 3516B, like Cat generators, is tested in accordance with the load steps outlined in with ISO 8528, Part 5.
    Q. Are Cat generators easy to install?
    A. Cat generators can be configured with a number of options for ease of installation.
    Q .Does Cat' have much experience with electric power generation?
    A. Cat has over 80 years experience with on-site and portable power and has shipped millions of generators to customers around the world.
    Q. Does Cat offer generators that support my Sustainability goals?
    A. Cat offers generators that can run on a number of renewable fuels including HVO, biodiesel, landfill gas, sewage gas and more.
    Q. Will this generator be able to provide emergency power on hot summer days?
    A. Most Cat 3500 Series generators can operate in ambient temperatures up to 50°C (122°F), reliably providing power when it is needed.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Cat Electric Power now has two tools available for sizing gensets in any application. 

Size Now
genset sizing
genset sizing

Data Centers 

You have a commitment to keep. You’re trusted to protect the information businesses rely on, safeguard online transactions and store critical content for easy access.

View Data Centers page
data centers
data centers

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service, and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.