Power Chords

Sommerbris Music Festival
Sommerbris Music Festival

Sommerbris Music Festival Relies On Cat® Hybrid Energy Solution To Power The Show

Customer:   Sommerbris Music Festival

Location:   Kristiansand, Norway

Customer Business Issue:   Reliable rental power that combatted noise requirements and met EU Stage V emissions standards.

Solution:  1320 kVA hybrid solution including lithium-ion energy storage integrated with two Cat® XQP310 mobile diesel generators.

Cat® Dealer:  Pon Energy Rental

of

The outdoor amphitheater on the tiny island of Odderøya lacks the power needed for music gear, speakers and amps, stage lighting, and other production equipment.

of

Long before the artists arrive on stage, the gensets operate to fully charge the battery packs, which then supply power at about the noise level of a vacuum cleaner for more than eight hours of performances each day.

of

The hybrid system has performed flawlessly at every Sommerbris festival, and organizers have chosen Pon Energy Rental again to support the event again in June 2024.

of

Sommerbris has quickly grown into one of Scandinavia’s premier multi-day concert events, attracting more than 26,000 attendees over two days.

POWER NEED

In a few short years, the Sommerbris (Summerbreeze) music festival has quickly grown into one of Scandinavia’s premier multi-day concert events, attracting more than 26,000 attendees over two days. The outdoor amphitheater on the tiny island of Odderøya is in a recreation area lacking the power needed for music gear, speakers and amps, stage lighting, pyrotechnics, video displays, control boards, and other production equipment. Festival organizers required a temporary solution that delivered the energy needed in an environmentally friendly way and didn’t overshadow the performances.

SOLUTION

Pon Energy Rental, the local Cat® dealer, designed and delivered a mobile hybrid power solution that supplied up to 1320 kVA of power for Sommerbris. It included two lithium-ion battery packs, each supplying up to 350 kWh of energy, as well as two Cat XQP310 mobile diesel generator sets. Both products are EU Stage V compliant, which is one of the world’s toughest emission standards for non-road mobile machinery, by reducing particulate and NOx emitted by engines.

Long before the artists arrive at the stage, the generator sets operate for about an hour and a half to fully charge the battery packs, which then supply power at 60-85 decibels—about the noise level of a household vacuum cleaner—for more than eight hours of performances each day. If the power requirement exceeds the capabilities of the batteries at any point, the generator sets are configured to start automatically and take over the load for as long as needed.

“This battery pack is very popular with festivals and other events that use a stage,” said Olav Austad, sales engineer for Pon Energy Rental. “We use power lock connectors both in and out of the battery pack to accommodate most stage setups and allow us to deliver the right connection from the battery.”

RESULTS 

The power system has performed flawlessly at every Sommerbris festival, and organizers have once again chosen Pon Energy Rental to support the latest edition of the event this June.

“We used Pon Energy Rental precisely because this is what they do, and they’re good at it,” said Heine Strømme. “Why choose someone new when we can choose a supplier that we know works and delivers good solutions every time?”

For more information on Cat Electric Power rental solutions, visit cat.com/rentalpower.

Download the Power Profile

Featured Products

  • rental

    Generator for Hire

    From compressed air to temperature control, we offer rental power solutions for your temporary needs.

    Learn More
  • XQP310
    Rating Prime
    310 kVA
    310 kVA
    Frequency
    50/60 Hz
    50/60 Hz
    Voltage
    220 - 480 V
    220 - 480 V

    XQP310

    This XQP310 generator set is EU Stage V emission standard capable. Each model delivers increased flexibility by easily switching between 50 and 60 Hz, which allows one machine to satisfy varying load requirements across diverse regions and applications including mining, manufacturing, oil and gas and construction.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Caterpillar Electric Power now has two tools available for sizing gensets in any application. 

Size Now
genset sizing
genset sizing

Rental Power

Cat Rental Power delivers clean, reliable, fuel-efficient gensets whenever and wherever you need them. 

View Rental Page
Rental
Rental

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.