Environment, economy, and energy

ebi
ebi

Cat generator sets use biogas to power over 7,000 homes

Customer: EBI Énergie

Location: Saint-Thomas, Québec, Canada 

Customer Business Issue: Renewable power generation using landfill gas processing 

Solution: Seven Cat® 3520C generator sets, CHP and switchgear 

Cat® Dealer: Hewitt Energy

of

Located 40 miles north of Montreal, EBI Énergie’s Saint-Thomas cogeneration facility provides Québec-Hydro with electricity derived from landfill biogas.

of

“These engines perform very well–it’s perfect for us,” said Turcotte.

of

Hewitt Energy also provides EBI Énergie operations personnel with service training, equipment support and parts maintenance.

of

EBI Énergie

of

Caterpillar customer and Canadian landfill management company, EBI Energie, explains why they worked with local dealer, Hewitt, to construct a 10MW LEED Platinum renewable CHP energy plant. www.catgaspower.com

Power Need

Through anaerobic digestion, biogas can replace natural gas as a renewable fuel source, providing numerous benefits to the environment, economy and energy market. Not only does biogas help reduce greenhouse gas emissions, it also generates reliable power at a fraction of the cost of traditional power sources.

As the biogas-to-energy formula became more efficient, the Canadian government passed a mandate to promote the generation of green electricity to reduce greenhouse gas emissions. As a result, electric power generation suppliers began working with government utility officials to create more sustainable options for electricity.

In 2010, Hydro-Québec–a state-owned utility in Québec, Canada–took the movement one step further by issuing an invitation for bid (IFB) for 125 MW of electricity derived completely from biomass. At the time, Québec did not have many renewable energy projects that could support such a large greenenergy mission.

Solution

In 1999, EBI Énergie, a waste processing company, installed its Dépôt Rive-Nord landfill facility to capture and burn off landfill gas to control the amount of methane gas released into the atmosphere. In 2003, EBI Énergie installed a gas treatment plant to turn the biogas into a renewable gas fuel for injection into the local gas pipeline. In 2010, after seven years of successful operation of the gas treatment plant, EBI Énergie won the IFB and signed a 25-year agreement with Hydro-Québec to produce 9.4 MW of renewable electricity through 2036 using excess biogas not already being sold to into the pipeline.

“Québec-Hydro asked us to guarantee capacity, and their requirements were strict,” said Luc Turcotte, EBI general manager. “We were able to demonstrate that we will have enough landfill gas to produce the required amount of electricity for 25 years. It was a good opportunity for us.”

Located 40 miles north of Montreal, EBI Énergie’s Saint-Thomas cogeneration facility provides Québec-Hydro with electricity derived from landfill biogas. Using a sophisticated process, landfill gas is gradually transformed into pipeline quality gas through a combination of dehydration, compression, filtration and membrane separation. The Saint-Thomas cogeneration power plant takes excess fuel from the gas treatment facility before it is stripped of carbon dioxide and injects it into the pipeline. The facility is unique to Canada, representing the only location in the country where biogas is used both as a renewable pipeline fuel and a source of renewable electricity.

At the cogeneration plant located less than a mile from the fuel processing facility, EBI Énergie pumps 4,500 standard cubic feet of methane per minute to six Cat® G3520C gas generator sets that convert the gas to electricity. A seventh unit serves as a swing generator. The G3520C generator sets are specifically designed to operate on biogas fuel.

EBI Énergie also required a fully automated facility that could be operated remotely. Local Cat dealer Hewitt Energy developed the SCADA control interface, which includes mobile capabilities, for the automated system. Operators can restart the plant using an iPhone app that connects to the SCADA system for engine monitoring in real time.

“It gives us a lot of flexibility to operate the plant, and it gives some comfort to the operator,” Turcotte said. “They are not tied to the plant, and yet are able to interact when required.”

Hewitt Energy also provides EBI Énergie operations personnel with service training, equipment support and parts maintenance.

“The main thing that we considered was the service aspect,” said Turcotte. “We plan to be in business for at least 25 years, and we want to have a reliable partner. It was clear in evaluating the quotations that the after-sale service and the parts support set Hewitt apart. If we have a problem on Christmas Day or January 1st, we know that Hewitt technicians will be available to assist us.”

Results

Since July 2012, when the Saint-Thomas plant began producing electricity, the Cat generator sets exceeded uptime targets and have operated at 99.9 percent availability, producing enough energy to power more than 7,000 homes.

“These engines perform very well–it’s perfect for us,” said Turcotte. “When we started the project, we all knew that generator performance was a key to success.”

The Saint-Thomas facility is pending approval as a Leadership in Energy and Environmental Design (LEED) Platinum facility–the highest rating in environmental engineering by the U.S. Green Building Council. The plant recovers aftercooler and jacket water heat from the engines to heat leachate treatment ponds in colder months. The microorganisms require a specific temperature for breaking down leachate that is collected and treated before being released into the environment. Without the heat recovery aspect, the facility would not be eligible for platinum certification.

“We are using the energy from the engine to heat the building, and also to heat the leachate,” said Turcotte. “At this point, we are recovering only 13 percent of the waste heat, so when it makes sense to expand, we’ll be looking to Hewitt for a combined heat and power solution to improve efficiency.”

Download the Power Profile

Featured products

  • Cat Switchgear
    Configuration
    IP4X
    IP4X
    Operating Temperature
    35 °C / 40 °C @ 1 hr, option for 0…50 °C (32…122 °F)
    35 °C / 40 °C @ 1 hr, option for 0…50 °C (32…122 °F)
    Standard Widths
    600 mm for ABB Emax2 E2 1600 - 2500A. 750 mm for ABB Emax2 E4 3200 - 4000A. 1200 mm for ABB Emax2 E6 4000 - 6300A.
    600 mm for ABB Emax2 E2 1600 - 2500A. 750 mm for ABB Emax2 E4 3200 - 4000A. 1200 mm for ABB Emax2 E6 4000 - 6300A.

    Cat Switchgear

    Cat Paralleling Switchgear is the perfect complement for the control and distribution of your emergency power. Modular and Customizable, our gen switchgear can be designed with protection and control architecture.

    Learn More
  • G3520C
    Continuous Rating
    2050 ekW
    2050 ekW
    Fuel Type
    Natural Gas, Biogas, Coal Gas
    Natural Gas, Biogas, Coal Gas
    Maximum Electrical Efficiency
    40.10%
    40.10%

    G3520C

    From natural gas-fueled combined heat and power (CHP) systems and emergency power for facilities, to renewable biogas energy to support the local grid, or electricity generated from coal mine gases, Caterpillar has a wide range of reliable gas power solutions.

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Cat Electric Power now has two tools available for sizing gensets in any application. 

Size Now
genset sizing
genset sizing

Landfills

Power your world with sustainable practices. Cat generator sets are designed to collect, clean and run on harmful gases produced by landfills. It’s reliable power that promises to reduce your environmental impact.

View Landfills Page
Landfills
Landfills

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.