Converting Waste Gas
Into Power

landfill
landfill

Cat® Gas Generator Sets Consume Landfill Gas and Create 22 mw of Power

Customer: Montauk Energy

Location: Orange County, California, USA

Customer Business Issue: Renewable power generation using landfill gas

Solution: Seven Cat® CG260 generator sets

Cat® Dealer: Cleveland Brothers Quinn Company

of

Seven Cat® CG260 generator sets consume landfill gas and create 22 MW of power 
to deliver to the residences, schools and businesses of Orange County.

POWER NEED

As a sprawling 725-acre operation, the F.R. Bowerman Landfill is one of the largest landfills in the United States. The landfill, located in Orange County, California, contains an estimated 31 million tons of waste.

When solid waste in a landfill decomposes, a natural by-product with high amounts of methane is released. This potent greenhouse gas can potentially affect global warming, climate change, ozone depletion and sea level rise, as well as having a negative impact on biodiversity. In order to better manage and reuse this onsite waste, Montauk Energy worked with Caterpillar Financial Services Corporation to develop and commission a $60 million, 113,000-square-foot, state-of-the-art renewable energy power plant to generate electrical power by capturing and conditioning the landfill gas.

“We’ve had successful gas energy landfill projects in Texas and Oklahoma, but this project was unique not only for its immense size but also for the strict emission requirements in place in California,” said Dave Herrman, CEO and President of Montauk Energy.

The Bowerman project is subject to regular inspections from the California Integrated Waste Management Board and the Board’s local enforcement agency, the California Regional Water Quality Control Board, in addition to the South Coast Air Quality Management District to ensure compliance with those regulations.

“With every new project, we look to leverage technology and innovation to increase efficiency and productivity with less impact on the environment and help our customers do the same,” added Patrick Barrett, a territory manager with Caterpillar.

In order to convert the waste into a renewable resource, Montauk Energy required generator sets with gas cleanup and emissions reduction technology to meet stringent standards.

SOLUTION

Montauk Energy worked with Cat dealer Cleveland Brothers to develop a sustainable solution for converting waste from the anaerobic digestion process into renewable energy. Seven Cat CG260 generator sets with reciprocating engines were supplied to create 22 MW of electricity.

“By law, the landfill gas must be flared because it can’t be put directly into the atmosphere as methane, however, now it becomes wasted energy. We were approached to capture it and generate electric power for the residences, schools and businesses of Orange County, California,” said Kurt Hertzler of Cleveland Brothers.

Due to the strict emission standards in California, the supplied generator sets feature technology designed to help the operation meet all local, state and federal air quality requirements. A fuel cleanup system treats the landfill gas to ensure it stays within acceptable limits of the engines, while selective catalytic reduction (SCR) and oxidation catalyst units were installed on each engine exhaust system to specifically reduce NOx, CO2 and VOC emissions.

“Beyond this essential balance-of-plant equipment, the generator sets are also built with drop-over enclosures to dampen noise. It was important to lessen the noise impact on nearby residential neighborhoods,” added Hertzler. “The enclosures also allowed us to create a very compact site, which helped. Although the landfill is vast, the space for equipment is actually quite limited.”

By selecting the large-scale CG260 generator sets, Montauk Energy ultimately required fewer units, thus lowering installation and maintenance costs.

RESULTS

As the largest gas-fueled reciprocating engine project in California, Montauk Energy is committed to helping the people of Orange County discover new ways to process and more efficiently use landfill gas.

The seven Cat CG260 generator sets add 160,000 megawatt hours annually to put into the grid, which is enough energy to power 26,000 homes. In addition, the generator sets and associated emissions controls prevent approximately 53,000 tons of CO2 emissions annually.

“This is the largest project of its kind utilizing landfill gas that combines gas cleanup, largescale Cat reciprocating enginegenerators and SCR technology to meet strict emission requirements,” Herrman stated. “The result is efficient operations with high online availability, coupled with ample and steady gas supply from the landfill, to ensure reliable production of renewable energy and all its benefits 24 hours a day, 365 days a year.”

Montauk Energy relied on Cleveland Brothers to develop, deliver and commission the project while Quinn Company will provide service for the plant under a 20-year long-term service agreement to ensure the plant is operating at peak levels for years to come.

“While the emission requirements were a considerable factor in this project, it was much more than simply meeting those obligations. A close collaboration between Montauk Energy, Cleveland Brothers and Quinn Company delivered the first successful gas-to-energy facility with sophisticated clean-up systems with SCR and oxidation catalysts to the market,” added Barrett.

Download the Power Profile

Featured Products

  • Gas Generator Sets

    Gas Generator Sets

    Cat industrial and commercial gas generator sets, at ratings from 100 to 4,500 ekW (100 to 4,500 kVA), operate on natural gas and a wide range of other gaseous fuels including biogas, landfill gas, coal gas and propane..

    Learn More

Electric Power products

Any size or shape. In any regulatory environment. When you need power, Caterpillar is equal to the challenge. Our generators are used in a variety of applications.

View Electric Power products
electric power
electric power

Generator Set Sizing Calculators

Cat Electric Power now has two tools available for sizing gensets in any application. 

Size Now
genset sizing
genset sizing

Landfills

Power your world with sustainable practices. Cat® generator sets are designed to collect, clean and run on harmful gases produced by landfills. It’s reliable power that promises to reduce your environmental impact.

View Landfills Page
Landfills
Landfills

CAT DEALERS MAKE THE DIFFERENCE

Your Cat dealer is committed to maximizing your success, helping you get the most out of your operations with site-level solutions, service and support.

CONNECT WITH YOUR DEALER TODAY
dealers
dealers
warning

Internet Explorer users may experience issues with certain features of our site.
Please try a current version of an alternate browser (i.e. Google Chrome, Microsoft Edge, Mozilla Firefox) for the full Cat.com experience.